Other Parts Discussed in Thread: AMC7820
The datasheet for AMC7820 shows on Page 6 that the rise time and fall time of the clock signal for the IC has a maximum rating of 30ns.
1. In a continuous mode of operation of the chip what will happen if the rise time increases beyond 30ns.
2. Is there a possibility that the chip will be damaged?
3. Will keeping a buffer for the SPI lines help. If so what should be the criteria to select such a buffer.?
4. Is it possible to provide SPI lines to multiple AMCs if the rise time of the SPI is kept within 30 ns?