Other Parts Discussed in Thread: CCSTUDIO, TM4C129XNCZAD, MSP430G2553
I got the new GA version 6.0.0.190, I was in try with beta release 00157.
Environment Linux Mint, on Cinammon 64Bit on a Vaio SVS1511C5E, Windows removed due to incompatibility with Linux and XP too, 8GB ram I7 NVidia. As many others I don't like Unity and everithing resemble M$ policy of imposition, so I searched for what is simple and productive.
I never got a package compiled on this new PC, I installed version 5.5 of CCstudio with a lot of problems, I ported all is Linux dependent to this platform, I ported all Altera code, but still no chance for CCStudio.
I try'd Beta release CCS6.0.0.00156, some troubles with mklib I never found and not mklibs on Linux, I was on try to complete library rebuild but on forum I read of this new release version CCS6.0.0.00190.
On Install reported some Library missing, (libgnome and two others) installation run't fine and CCstudio open in the new graphic version...
From beta release are missing view perspective useful to switch from editing to deug or building, but may be some better is in place, I read only 6.0 is now supported :((( Is this M$ policy of sell new version and stop productivity of users? Of much time is needed to solve everything is on new version and how many time is required to new learning curve of a new environment??
And in a production tree how much impact the new problems where from new version? Is this a good policy about what is developed on old version?
5.1 required a week to discover double stack setting and just one was working....
5.4 from 5.1 experience got working in a few hours (Old pc AMD 64 bit based Ubuntu 10.04 32 bit)
5.5 never I got a working on this new pc, still everything is mantained on old pc
6.0 Beta after few hour struggling got at a linking error stage where compiler reported libc.a not found... Simple project got compiled fine.
6.0 GA.... fresh installation, imported again new project and noooo not again a worst than I never see, a new NIGHTMARE!!!!!
Everything I try to modify same response, no build no touch no chance....
TIVA support disappeared so I on ARM menu is not possible build for....
CCstudio was on schedule to buy..... When can be a ready for production tools on TIVA and MSP series? Tomorrow I also try import C2000 code, My wish is to migrate from old pc to this new and have a full version working compiler.
( note: I try download Image late, now I got many time error on download)