Can't connect to my hardware anymore:
IcePick_C: Error connecting to the target: (Error -241 @ 0x0) A router subpath could not be accessed. A security error has probably occurred. (Emulation package 6.0.228.0)
Test Connection shows:
[Start: Texas Instruments XDS2xx USB Debug Probe_0] Execute the command: %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity [Result] -----[Print the board config pathname(s)]------------------------------------ C:\Users\ARMINI~1\AppData\Local\TEXASI~1\ CCS\ti\0\0\BrdDat\testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 560/2xx-class product. This utility will load the program 'xds2xxu.out'. The library build date was 'Apr 28 2016'. The library build time was '02:18:13'. The library package version is '6.0.228.0'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. The controller has a version number of '13' (0x0000000d). The controller has an insertion length of '0' (0x00000000). This utility will attempt to reset the controller. This utility has successfully reset the controller. -----[Print the reset-command hardware log-file]----------------------------- This emulator does not create a reset log-file. An error occurred while hard opening the controller. -----[An error has occurred and this utility has aborted]-------------------- This error is generated by TI's USCIF driver or utilities. The value is '-241' (0xffffff0f). The title is 'SC_ERR_ROUTER_SECURE_SUBPATH'. The explanation is: A router subpath could not be accessed. A security error has probably occurred. [End: Texas Instruments XDS2xx USB Debug Probe_0]
Before this happend, I cleared and programmed the internal flash within my application.
Is it possible to destroy the CC1310 that way?
Regards
Armin