Part Number: LAUNCHCC3220MODASF
Other Parts Discussed in Thread: CC3200, CC3220SF
Tool/software: Code Composer Studio
Hi,
I've been developing with the CC3200 with great success but now we are changing to the CC3220.
So, I am now using CCS v7 and the new cc32xx_sdk_1_40_01_00
I'm stuck trying to import example code into CCS.
I get the Device is either 'null' or is currently not recognized by CCS error.
I then tried to create a new CCS Project and when I look at the long list of target devices I don't know which one to use. I don't see any with CC3220 in the name. I suspect that's a problem.
I tried Help/check for updates, but it says there are no new updates.
Can you tell me what I need to do to enable support for the LAUNCHCC3220MODASF?
Thanks,
Chuck