This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connection between Raspberry pi or NVIDIA Jetson Nano with DLP®︎ NIRscan™︎ Nano Evaluation Module



Hi!,

I'd like to know ir if possible to connect a DLP® NIRscanTm Nano Evaluation Module between Raspberry PI4 or NVIDIA Jetson Nano?.

There are some examples about that?

If the connection could be possible, which communication port must be used? (USB, SPI, MIPI, Bluetooth)?

Which software with or without GUI interface could be used with Linux Ubuntu? maybe with Raspbian (for raspberry pi).

Thanks a lot!