This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC: About changing the external thermistor.

Part Number: DLP3010EVM-LC
Other Parts Discussed in Thread: DLPDLC-GUI, DLP3010, DLPC3478, DLPA3000, DLP3010LC, DLPA2005

I am changing the thermistor into another one on the display board of DLP3010EVM-LC.

I have read the following thread, and I have understood that I need to change the lookup table installed to the firmware to support the new thermistor with different B-constant.

https://e2e.ti.com/support/dlp-products-group/dlp/f/dlp-products-forum/965549/dlp4710evm-lc-about-the-temperature-acquisition-command/3579387?tisearch=e2e-sitesearch&keymatch=DLP%20thermistor%20B-Constant%20LUT#3579387

So, my question is;

     How can I install a new lookup table for thermistor into the firmware ?

     (Does the DLPDLC-GUI have a function to change the lookup table ?)

Regards,

Hiroyuki Oka

  • Hello Hiroyuki Oka,

    To update this B-constant you will need a new firmware image for the EVM. I will talk with the team about the best way to create this image and then post back.

    Best regards,

    Arthur Brown

  • Dear Arthur Brown

    Thank you so much.

    I will wait for the post back.

    Best regards,

    Hiroyuki Oka

  • Hello Hiroyuki Oka,

    Can you share the data sheet of the thermistor you are using? if the data sheet is not available I need the thermistor resistance and B-constant.

    I will make the firmware for you and then share a download link from our secure sever. I sent you a friend request so I may message the link to you.

    Best regards,

    Arthur Brown

  • Dear Arthur Brown

    Thank you so much for your suggestion.

    But now I am using two following firmwares;

        (1) firmware (v7.3.2)

        (2) test-fixed firmware (v8.1.100) which is supplied by Mr. Philippe Dollo and Mr. Mayank Khandelwal.

    ----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
    DLPC3478PROM: Configuration Fimrware for DLP3010+DLPC3478+DLPA3000 chipset
    Release: 8.1.100
    Date: 04/22/20
    ----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
    General Description
    ----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
    This is a test build firmware compatible for DLP3010EVM-LC. Kindly use this firmware to check if it addresses the issue reported in the following e2e ticket
    - e2e.ti.com/.../3669759

    Kindly note that this is a evaluation build and not a production build. Use it for testing purposes only.
    ----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

    As I mentioned in https://e2e.ti.com/support/dlp/f/dlp-products-forum/989160/dlp3010evm-lc-an-issue-with-firmware-of-ver-8-0-0/3669759#3669759, 

    DLP3010EVM-LC (including DLP3010 chip) needs firmware (v7.x.x).

    on the other hand, DLP3010EVM-LC (including DLP3010LC chip) needs firmware (v8.x.x).

    So I'm happy if you let me know how to change the thermistor's lookup table in any firmware.

    For the time being, I will tell you the external thermister's information I use.

    The Product number of the thermister is "104JT-025".

    The following link is the datasheet of the thermistor I am using.

        docs.rs-online.com/.../0900766b80ff55d0.pdf

            --> The thermistor resistance is 100k, and B-constant of "104JT-025" is 4390K.

    Best regards,

    Hiroyuki Oka

  • Hello Hiroyuki Oka,

    unfortunately you will not be able to update the LUT with the GUI. we will need to do it and then give it to you.

    I will create you a firmware with updated LUT for v7.4.2 (for DLP3010) and for v8.1.1(for DLP3010LC)

    I have a few questions about the firmware.

    1) you mention DLPA3000, but the DLP3010EVM-LC uses the DLPA2005. has the PMIC been changed?

    2)Does your firmware have any other changes different from stock EVM firmware?

    thank you and best regards,

    Arthur Brown

  • Dear Mr. Arthur Brown,

    Thank you so much for the kind suggestion.

    And I'm sorry for the late reply.

    I found an external thermistor whose B-constant and resistance are the same as EVM's thermistor's.

    And I will use it so that I can use the public EVM firmware.

    Thenk, this issue has been resolved for me.

    Thank you for your great help.

    Best regards,

    Hiroyuki Oka

  • Hiroyuki-san,

    Thanks for your confirmation.

    Regards,

    Mayank