This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC410EVM: Unable to use the Discovery D4100 Explorer GUI with the example appsfpga desgin

Part Number: DLPLCRC410EVM
Other Parts Discussed in Thread: DLP7000,

Hi,

I have a customer who is working with DLPCRC410EVM and encounter some problem with his set-up.

Please see below with his query and I hope you can help him to his problem. Thank you very much.

(DLPLCRC410EVM DLP7000) Hi, I am trying to change the application FPGA. So I constructed an ISE project with the DLP(R) Discovery 4100 Applications FPGA Pattern Generator Source Code. But after programming the FPGA, the image load and reset commands will not update the DMD to display the image, the DMD just flickers. I think the problem is in the USB_IO_CLK.vhd module, but I don't know exactly, since the USB communication is done by the Cypress chip.

Best Regards,

Ray Vincent