This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP660TE-SW: VX1 get infomation on DLP composer

Part Number: DLP660TE-SW
Other Parts Discussed in Thread: DLP660TE, DLPC4422

Hi  TI Engineer,

When using  DLPDLCR660TEVM and DLPLCRDC4422EVM  development board, We want to add XPR function.

Use environment

Hardware: DLPDLCR660TEVM ,DLPLCRDC4422EVM and usb cable

sofeware:  DLPC4422 GUI 1.0,  DLP660TE_Chipset_Firmware_v9.0(DLP660TE_chipset_FPGA.rpd and Flash_DUAL_DLPC4422_DLP660TE_LED.img) 

The Vx1 uses item 2 for 4K and item 8 for 2.7K, but the 4422 EVM board gets the same parameters in Autolock page as the attached pictures.

         Autolock of another setting (2.7K, 120Hz) gets no value. Why?

         Could you give feedback to Vx1 setting?  Can you tell me the meaning of each parameter?  What is the correct operation process?

         Looking forward to you