This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPNIRNANOEVM: DLPNIRNANOEVM

Part Number: DLPNIRNANOEVM


Hello!

I recently received a DLP NIRScan Nano EVM device (900-1700 nm range), so I have a few questions:

I installed NirScan NANO GUI v1.1.9, using the device, I got 3 spectra in the software interface (Intensity, Absorbance, Reflectance), and after scanning the sample, I got the output of the absorption (AU) and Reference Signal (unitless), Sample Signal (unitless) , but not the REFLECTANCE.
I need reflectance output for my research work (if the software shows spectra, that means I can also get reflection output, right?)

So how can I get the reflectance output from this device?


*** I'm doing research, analyzing the reflection spectra from PET bottles. From the absorption coefficient, it shows only noise, even after a new calibration, it shows an insignificant value, most of the zeros (maybe I can make a mistake when calibrating)


Waiting for your reply,

Nazym