Hi,
I'm testing the EVM by connecting it to the Raspberry PI and setting the display mode to the 960x540@240hz.
There were several issues when setting up including the insufficient current in the GPIO pins and the FPGA misalignment with the video data.
Today, I have displayed something at 240hz on the Raspberry PI via the EVM and found another problem.

https://www.youtube.com/watch?v=LYha7v6h6U0
The reason why I recorded the video was that I felt the screen is torn even though the frame rate is set to 240hz and also reported to follow the vsync.
I used the iPhone slowmo and also the vsync-connected hardware camera : both results were the same. The screen is torn.
When we look at the captured video, we can see that the gears are torn in the middle.
I used the famous sample openGL program "glxgears" (only modifying the gear's rotation axis, to see the issue more clearly) which renders images while vsync enabled by default.
What could be the cause of this problem?
Could this be another FPGA misalignment with the video data issue—how can I fix this problem?
Thank you.