Other Parts Discussed in Thread: DLPC3478, DLPA2005
Dear Expert
Our product USES dlp3010lc+ dlpc3478+ dlpa2005. Our use scenario is a trigram in modeon of optical control and internal pattern mode.
The pin mapping between dlpc3478 and dlp3010lc is option 1.
The led connection on the hardware is the following: Green: Red. The current firmware 8.0.0 is the default starting power current at 1498,1498,1498. Please change it to 600, 600, 600.
The i2c address: using dlp3010lc evm default, it should be 36h.
4. uvlo Settings range: 2.3v.default minimum. Deglitch time: 100us.
Start the picture, see chart start3.png.
Change the transient-current limit settings3 leds. Three sw all make energy, ireg_ilim<. 3:0>g; Set to 1100 2538ma-.