This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: Firmware update troubles

Part Number: DLP4710EVM-LC
Other Parts Discussed in Thread: DLPC3479

Hello, I've tried to update my DLP4710EVM-LC firmware to dlpc3479_fw_8.1.0.img. When flashed the EVM can't connect to I2C anymore. The reason for the update was to hopefully correct a color shift between 127 and 128 in RGB.

Thank you for your help,

Justin