Part Number: DLPDLCR4710EVM-G2
Other Parts Discussed in Thread: DLP4710EVM-LC
Dear experts,
I use the chipset in DLPDLCR4710EVM-G2 as a spatial light modulator to shape a femtosecond laser (1 kHz, 100 fs, 400 nm). The input to the EVM is a 1-bit depth binary image, a ring pattern, through the HDMI port. I succeeded to see the ring pattern, but there is a blinking background at some frequency which is not desirable for my application. Do you have any solutions to remove the background? Thank you very much.


Best Regards,
William