This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC300: Save 608*684 pixel images to DLPC300 firmware

Part Number: DLPC300

Dear engineer, I have some questions to ask you。I see that the DLPC300 firmware can store 4 splash screens index, but their pixels are 427*240 of 24-bit RGB. I need to realize the function of Sequencer Control, but it requires that the pixel of the picture is 608*684, so is there any way to save the picture with 608*684 pixels to DLPC300 firmware DLPR300PROM_v1.0.bin?
I mainly want to realize the function of Sequencer Control, the pictures will be uploaded through nor flash connected with DLPC300, and the 608*684 pixel pictures will be merged into the firmware or put into other places of flash. How to transfer them to DLPC300? I would like to ask if there is any way