Other Parts Discussed in Thread: DLPC3479
Hi,
I want to project a 1-bit image at a high frame rate with the DLP4710EVM-LC.
I found that images can be displayed at 1440Hz by using 1-bit monochrome mode.
Then, is it possible to update the projected image from the PC at 1440 Hz?
Or, since the transfer rate of HDMI is 60Hz, is it necessary to combine 24 frames into a single image and transfer it?
In this case, projection images are generated every 16ms.
best regards,
murakami