Other Parts Discussed in Thread: DLPC910, DLPC900, , DLPLCR65EVM, DLP6500FYE, DLPLCRC900EVM, DLPLCR65FLQEVM, DLPLCRC910EVM
Dear all,
I have a question regarding which controller to choose for my application when using a DLP6500FLQ DMD: DLPC900 or DLPC910.
One main criterion for my application would be at what (effective) rate I can display larger pattern sequences of 1bit patterns (>10000 patterns). The maximum number of pre-loaded images is 400, is this correct for both controllers? So I would have to transfer patterns from a PC to the DMD. What would be the best way to do this regarding a high effective rate? Transfer via USB or via a video stream?
Could you clarify this questions a bit, also by comparing the DLPC900 and DLPC910 controllers? Which evaluation or development boards do I need?
Thank you in advance.
Best regards,
Pascal