When I first power on the DMD (DLP 7000) with the on switch, I see a horizontal line across the display, even as it cycles through test patterns without connection to a computer. I am using the DLP Discovery 4100 kit and I've switched boards and flex cables with known working ones, which have not changed anything. Loading images/resetting/clearing and pressing the hardware reset (SW2) has also not removed this line. Additionally, pressing SW3 (manually float the mirrors) does remove the line so the mirrors themselves seem to be working correctly.
It previously did not do this so I'm not sure what connections, if any, to test and what other ways I can troubleshoot.
Thanks!