Other Parts Discussed in Thread: DLPC410
We have in-hand a half dozen recently purchased 'C410 EVM boards. These boards were delivered without the FPGA config prom footprints populated (U8 and U10) and the board layout has been changed compared to prior board version. Most obviously, the layout now has two additional pin headers (J19 and J20). Per advisory notice, it is understood that the DLPR410 prom is obsolete and unavailable, and I assuming that the added headers are to be used as a workaround to substitute the serial flash parts described in the advisory. All good, if true, I suppose. Problem is that we have customer delivery commitments for these units and there is no published info available about these boards changes or info on how we can to bring them to life. And, there was no warning or cautionary advice provided upon purchase to indicate that these boards would be unusable out-of-box. I have looked everywhere on ti.com and cannot find the updated design files or any related info. Am I missing something?