Part Number: DLPDLCR3310EVM
"When I was using the DLPDLCR3310EVM today, the screen of the computer can be displayed normally when I just turned it on (connected with an HDMI cable), but it suddenly fails to display the screen after about 1-2 minutes, and it can be displayed normally after I turn it on again, but it is also about 1 -After 2 minutes, the screen cannot be displayed suddenly, how can I troubleshoot the problem?"
This is the problem I had last time. I paused the test for some reasons, and now I’m back to continue solving it.
Last time you gave me some methods to check first. Here are the results I saw:
A1-4: I didn't use software at first, but simply used the projector as the second screen of my computer, but I encountered this situation. Then I connected the software "DLP LightCrafter Display v7.4 - 3310EVM" provided on the TI website, and Didn't see any error message telling me.And it happens in any mode, even if I just turn on the projector.
A5:I am using a standard power supply to drive the projector and I am sure there is no problem.
When I connected the power, both D1 and D7 were on (although the photo is unclear, I'm sorry), the "reset" light was on, and D5 was on after turning on the projection, and there were two other lights on (as follows) )
When the projection function fails after about 1-2 minutes, D1, D5, and D7 are all on, but the lights mentioned above change to the following
Please help me solve it, thank you