Other Parts Discussed in Thread: DLPC150
Hello, senior TI engineer, I have a problem when I carry out secondary development according to the NIR suite, and I hope TI will solve it, as follows:
I downloaded the schematic source file from the official website (2514151_NIRSCANNANO_DLPC150_BOARD_ESD. DSN) and the PCB source file (23327-04_NIRscanNANO_DLPC150_board), the data of the two files should be consistent; I EXPORTED THE SCHEMATIC TO netlist AND IMPORTED THIS netlist FILE INTO THE PCB SOURCE FILE, ONLY TO FIND THAT THERE WAS A PROBLEM WITH THE PCB SOURCE FILE, A LOT OF ERROR NETWORKS; Explain that the schematic and PCB do not match; This is just one of the schematic and PCB problems, and several other board schematics and PCB are also the same problems, I hope TI can provide the correct schematic and PCB files, thank you
The following is a PCB (23327-04_NIRscanNANO_DLPC150_board) that directly opens TI's official website:
The following uses the schematic diagram of TI's official website (2514151_NIRSCANNANO_DLPC150_BOARD_ESD. DSN) and import this netlist to the PCB source file (23327-04_NIRscanNANO_DLPC150_board):