Other Parts Discussed in Thread: DLP660TE, , DLPC4420, DLPC4420AEVM
HI Team.
Our company is producing new products using DLPC4422 and DLP660TE.
I designed th board referring to the DLPLCRDC4422VM Board.
After producing the board, I proceeded with the program as follows.
1. install DLPC442xJTAG-1.0-windows-installer.exe
1.1 Detect Chain - UM232H Rev 1.0
1.2 File select
-> Board File : BoardFile.brd
-> Flash Image To Write : bootloader_DLPC4422_dual.bin
1.3 Program OK and Verification OK
2. install DLPC4422-GUI-v1.0-Setup.exe
2.1 DLPC4422 GUI program execution.
2.2 File Selection
-> Flash Image File : DLP660TE_chipset_FPGA.rpc
-> Flash Type : Serial Flash
2.2 USB Reset OK
3. Program Download
3.1 Start Download
-> When i run Start Download, the following message is displayed.
4. Power On
4.1 When the power on, i confirmed that data was being read from the Flash Memory.
4.1 Power Status
-> All Power Is OK (1.8V, 2.5V, 3.3V, 1.1V etc)
4.2 Clock Status
-> Master Clock ; 20Mhz OK
-> Slave Clock : 20Mhz OK
-> OCLKA : 787Khz
-> PWRGOOD : HIGH
-> POSENSE : HIGH
-> MTR_ARSTZ : LOW ???
5. Questions
5.1 Is there a problems with the above process ?
5.2 In what cases does the following message appear?
-> " Error : Unable to enter device programming mode"
5.3 Are there any other signals we should check for ?
Please help me....
Thanks & Regards.
Kwangsam