Other Parts Discussed in Thread: DLPA2005, DLPC3478, DLP3010LC
Dear TI Members
I got two type of Firmware and release Note from TI site and checking pre-test items with DLP3010EVM-LC before developing the real sample.
Case1) DLP3010EVM-LC_Firmware_v9.0.1
Release Note : file:///C:/Users/rodin/AppData/Local/Temp/2e25bcd8-703f-4128-aebe-168fda3b64b7_DLP3010EVM-LC_Firmware_v9.0.1.zip.4b7/DLP3010EVM-LC_Release_Notes_v9p0p1.htmlDLP3010EVM-LC_Firmware_v9.0.1.zipDLP3010EVM-LC_Firmware_v9.0.1.zipInternal Mode Exposure time.pptx
Case2) FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v9p0p1
TI Recommended that it use FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v9p0p1 instead of DLP3010EVM-LC_Firmware_v9.0.1
Release Note : file:///C:/Users/rodin/Desktop/FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v9p0p1/FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v9p0p1.html
Q1) Why is mentioned difference exposure time and format for internal Mode?
Case 1 mentioned 5 type pattern mode with exposure time and pattern numbers but Case 2 mentioned exposure time without pattern numbers.
It is same v9p0p1 and chip sets such as DLPC3478, DLPA2005 and DLP3010LC
Q2) Can I use pattern type that was mentioned Sequence 14,15,16,17,18 with exposure time?
If I want to 10 patterns of 1 set , Is it possible?
Q3) What is used case 1 or case 2 Firmware and release note?
Thanks
Best & Regards
ES Kim