Other Parts Discussed in Thread: DLPC900, DLPLCR4500EVM, , TFP401, DLPC350
Dear all,
Like many before me, I am currently trying to get 120Hz video mode to run on our EKB DPM-E4500MKIIRGBHP.
CAn you confirm that 120Hz Video mode is functional?
I can confirm that I can set 120Hz 1200x800 or any other output using the Nvidia tools. As in the other threads below, video output is detected as 120Hz.
However, the framerate for anything but 60Hz is effectively 15Hz (see top link), even though sync seems to be correctly taken at 120Hz. Also in Video Pattern streaming mode, frame updates are not triggered at 120Hz as far as I can tell.
Is it possible that the effective rate is capped at 60Hz by the video receiver chip, as stated for the DLPC900?
It was suggested that this will be added in future firmware. Did this happen?
Best wishes
Tobias