Hi,
We have been trying DLP4500 with 1280x800@120Hz in Video Mode. (Firmware Version is 3.0)
But the projected screen is always updated slower than 60Hz and there are many frame drops,
whereas we have no problem with 1280x800@60Hz in Video Mode.
Are there any limitations to the frame data which can be output at 120Hz?
Can we get 1280x800@120Hz in Video Mode?
Our NVIDIA GPU display setting is customized exactly same as:
https://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/p/331370/1160989#1160989
and the pixel clock is below 150MHz which should be OK.
Also, we have already checked the following but were not able to find the right way:
https://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/t/499863
https://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/t/331370
https://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/t/312672
We are using: WIndows 8.1 Pro. NVIDIA Geforce Titan X, HDMI->mini HDMI
Best regards,