Hello
I am designing a laser processing machine using DLP7000UV.
We are currently in the process of creating and experimenting with a prototype.
We are verifying that diffracted light is generated in front of the imaging lens and is having a negative impact on the distribution on the workpiece surface.
Please refer to the attached PDF file for the results.
Contents of the PDF
P1: Equipment configuration
P2: Photo: Unevenness in front of the imaging lens
P3: Photo: Mirror on/off in front of the imaging lens
I have a few questions regarding this.
Q1. Is the unevenness in front of the imaging lens due to diffracted light?
If it is diffracted light, why does diffraction occur?
Is it due to the relationship between the DMD mirror structure and the laser wavelength used? The laser used is a multi-mode laser that uses light bundled with several laser diodes, so I thought that the wavefront of the light would be uneven and diffraction would be less likely to occur, but is this not true?
Q2.
If diffracted light occurs in front of the imaging lens (2), will it have a negative effect on the distribution on the workpiece surface (3)? Has such a thing been a problem in the past?
For example, the drop in output. Deterioration of distribution uniformity, etc.
Q3.
Is there a way to eliminate the diffracted light?
Is there a good optical design method to eliminate diffracted light?
Thank you for your advice.