DLPNIRNANOEVM: DLP NIRscan Nano EVM command reference

Part Number: DLPNIRNANOEVM

Tool/software:

Hello,

I need to build a separated aplication at python, which supports yours DLPNIRNANOEVM through the UART communication.
(I already can send commands /receive a proper answers through sreial port, bud I after that I must interpret the scan data blob through DLP Spectrum Library-and I can not find any python examples).

Have You got some ".py" exmples how to use a NIRNANOEVM and DLP Spectrum Library?

If no, can you point which libs /files should I use to prepare small external application which will made only:
PerformScanReadData()
spectrum.SetData()
spectrum.SaveToFile() functions?

I tried to find this in the GUI source, but it's a very large Cpp project and I can't isolate these functions properly.

Regards
Dawid