Other Parts Discussed in Thread: DLP4710LC, , DLPA3005
Tool/software:
Hello!
tri_out2 cannot be configured
The details are
tri_out1 configuration OK(8'h92 8'h02,8'h00,8'h04,8'h00,8'h00) (all values can be written normally)
tri_out2 configuration NG(8'h92 8'h03,8'h00,8'h00,8'h00,8'h00) (Slave does not answer when I write 8'h92)
Also, no other registers can be written.
We've checked the power-on timing. There's no problem. And test images can be output (register 05 is set to 01)。
When the iic continuously writes to the register, do I need to wait for a period of time after each write? What is the length of the wait?
Please help analyze it !
Thank you very much!