Other Parts Discussed in Thread: DLPC6540, , DLP471TP
Tool/software:
Hello, E2E Forums.
With the help of TI forum, I installed the bootloader and firmware on DLPC6540 (DLPDLCR471TPEVM).
I checked the connection in DLP EVM GUI and confirmed that the Splash image and other functions are working properly.
However, HDMI is not connected. When I press the 'Switch to External Video' button, it does not switch to the PC screen.
PC does not recognize HDMI port.
- When click the 'Switch to External Video' button, a splash image appears.
I used following files :
- 3312.DLPC6540_JTAG_FlashProgrammer
- DLP471TP_EVM_v3.2.2_MCU_FW4.5.0.img
- FlashDeviceParameters.txt
// Mfg MfgID LMfgID, Device DevID LDevID, Mb Alg Size #sec Sector_Addresses
"Micron", 0x0089, 0x0000000000000089, "MT28EW256", 0x227E, 0x000000000000227E, 128, 0, 0x1000000, 128, 0x0, 0x20000, 0x40000, 0x60000, 0x80000, 0xA0000, 0xC0000, 0xE0000, 0x100000, 0x120000, 0x140000, 0x160000, 0x180000, 0x1A0000, 0x1C0000, 0x1E0000, 0x200000, 0x220000, 0x240000, 0x260000, 0x280000, 0x2A0000, 0x2C0000, 0x2E0000, 0x300000, 0x320000, 0x340000, 0x360000, 0x380000, 0x3A0000, 0x3C0000, 0x3E0000, 0x400000, 0x420000, 0x440000, 0x460000, 0x480000, 0x4A0000, 0x4C0000, 0x4E0000, 0x500000, 0x520000, 0x540000, 0x560000, 0x580000, 0x5A0000, 0x5C0000, 0x5E0000, 0x600000, 0x620000, 0x640000, 0x660000, 0x680000, 0x6A0000, 0x6C0000, 0x6E0000, 0x700000, 0x720000, 0x740000, 0x760000, 0x780000, 0x7A0000, 0x7C0000, 0x7E0000, 0x800000, 0x820000, 0x840000, 0x860000, 0x880000, 0x8A0000, 0x8C0000, 0x8E0000, 0x900000, 0x920000, 0x940000, 0x960000, 0x980000, 0x9A0000, 0x9C0000, 0x9E0000, 0xA00000, 0xA20000, 0xA40000, 0xA60000, 0xA80000, 0xAA0000, 0xAC0000, 0xAE0000, 0xB00000, 0xB20000, 0xB40000, 0xB60000, 0xB80000, 0xBA0000, 0xBC0000, 0xBE0000, 0xC00000, 0xC20000, 0xC40000, 0xC60000, 0xC80000, 0xCA0000, 0xCC0000, 0xCE0000, 0xD00000, 0xD20000, 0xD40000, 0xD60000, 0xD80000, 0xDA0000, 0xDC0000, 0xDE0000, 0xE00000, 0xE20000, 0xE40000, 0xE60000, 0xE80000, 0xEA0000, 0xEC0000, 0xEE0000, 0xF00000, 0xF20000, 0xF40000, 0xF60000, 0xF80000, 0xFA0000, 0xFC0000, 0xFE0000,
I'm checking the circuit I made.
Is there a possibility that there is a problem with the software I used?
Is there a way to get the GUI to recognize HDMI?
I have one more question.
Is there a way to change the splash image? I want to change the image that is displayed when the projector boots up.
I need help from the TI E2E forum. Thanks.