Part Number: DLPLCRC964EVM
Other Parts Discussed in Thread: DLP991U, DLPC964, , DLPLCR99EVM
Tool/software:
Hi again team,
Context: I'm currently looking at designing a system aiming to minimise feature size of a lightfield at 395-405 nm. See here for more info. I've currently arrived on the DLP991U DMD in order to minimise mirror pitch whilst remaining in the UV spectrum. That has lead me to the DLPLCR99EVM/DLPLCRC964EVM combo, which seems acceptable for 405nm.
Question: The DLPC964 documentation leads me to understand that an external FPGA is required. Can this be avoided (and data loaded directly from a PC) if high-speed applications aren't being utilised? I'm happy to have only one pattern available, with a reboot & config adjustment required to change patterns, if that simplifies hardware/dev.
If one is required, the documentation recommends a AMD Virtex 7 FPGA VC707, which has been discontinued, leading me to the AMD Virtex 7 FPGA VC709. I'm not experienced with programming FPGAs/using Vivado, is this simply a matter of loading the VHDL code provided, modifying patterns via the BPG pattern txt files, and selecting via the TI-provided GUI?
Thanks again in advance,