Tool/software:
How to show the splash pattern?
I used the 9.5.1 project file and change the splash pattern to a resolution 1280 x 720 png file then build the image file.
After load the image file to the Light Engine, I used composer to show the pattern but is no OK and even can not recognize a pattern.
below is my step:
1.change to Splash Mode
2.write splash screen select to 0
3.write splash screen execute