Tool/software:
I am trying to drive the DMD using the DLP4620EVM. The DLP Composer project I previously received only allows resolution changes to 1220x610 or 1358x566. My current issue is that I want to display a completely filled screen using all the pixels of the DLP4620. Upon checking the datasheet, it states that for resolutions of 960x480 and 1920x960, the DMD diamond mirrors used can support 960x960. However, neither of these options can be selected in the composer at the moment.
For this reason, please provide a project file in which the resolutions of 960x480, 1220x610, and 1358x566 can be selected.
Furthermore, I want to use a resolution of 1920x960 with the DLP4620EVM system. How can I achieve this?