This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2021LEQ1EVM:[Support Request] How to Load Custom Images into DLP Composer Project

Part Number: DLP2021LEQ1EVM
Other Parts Discussed in Thread: DLP2021-Q1

Tool/software:

Dear [TI Support / DLP Team],

I hope this message finds you well.

I am currently working with the TI DLP platform, specifically the DLP2021-Q1 chipset, and I would like to project custom images through the system. To do this, I am attempting to use the DLP Composer software to configure a new sequence that includes a user-defined BMP or PNG image, and then build it into a flash image for deployment.

However, in the Composer environment I received, the option to create a new project appears to be unavailable, and whenever I attempt to add a custom image file, I receive an error stating that the file type is not supported.
Interestingly, default sample BMP images provided within the project do work correctly, which leads me to believe that the Composer version I have may be a restricted or preconfigured edition with limited functionality.

I would greatly appreciate your guidance on the following points:

  1. What is the proper procedure for creating a new sequence with custom image input using DLP Composer?
    (e.g., new project creation, image import, sequence mapping, flash build, etc.)

  2. What are the recommended or required image specifications and format constraints (e.g., color depth, resolution, compression) for successful use in Composer?

  3. If the Composer version I’m using is limited, could you please direct me to the appropriate full-featured version (e.g., DLPC137 or similar), along with download and installation instructions?

  4. Are there any specific Composer versions that are required or recommended for compatibility with DLP2021-Q1?

Thank you in advance for your support. I look forward to your detailed guidance so I can proceed effectively with my development and testing.

Best regards,

MYEONGJAE