This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would like to request two pattern sets as seen below.
PExT = 8333 us
Bit-Depth | # Patterns | Color |
8 | 9 | Green |
1 | 9 | Green |
1 | 1 | Red |
1 | 1 | Green |
1 | 1 | Blue |
And,
PExT = 8333 us
Bit-Depth | # Patterns | Color |
8 | 9 | Green |
1 | 10 | Green |
1 | 1 | Red |
1 | 1 | Green |
1 | 1 | Blue |
Thank you,
Cole
Hello,
I would still like the request the above pattern sets but also add the two below:
PExT = 8333 us
Bit-Depth | # Patterns | Color |
8 | 9 | Blue |
1 | 9 | Blue |
1 | 1 | Red |
1 | 1 | Green |
1 | 1 | Blue |
PExT = 8333 us
Bit-Depth | # Patterns | Color |
8 | 9 | Red |
1 | 9 | Red |
1 | 1 | Red |
1 | 1 | Green |
1 | 1 | Blue |
Thank you,
Cole
Hi Cole,
Should not be a problem generating the sequences, but please allow until the end of this week for us to post them.
Thanks,
Eric
Hello Cole,
The patterns should post to the following URL within a day.
http://software-dl.ti.com/dlp/embedded/catalog/dlp3000/dlp3000mbmc.html
Regards,
Eric
Hi,
I recently tried to use my MBMC:
9 x 8bpp G + 10 x 1bpp G + 1 x 1bpp R + 1 x 1bpp G + 1 x 1bpp B with Exposure = 8333us
and
9 x 8bpp G + 10 x 1bpp G + 1 x 1bpp R + 1 x 1bpp G + 1 x 1bpp B with Exposure = 10500us
Issue #1:
Parsing with the most recent GUI creates a black pattern for the R, G, B patterns.
Issue #2:
Parsing with an older parser seems to create white patterns where R, G and B should be. The issue I have is that when I use the .bin file everything is fine as it projects the Red, Green and then instead of Blue it projects Green again.
Has there been a change in firmware or the parser?
Can I get a new bin file generated for:
9 x 8bpp G + 10 x 1bpp G + 1 x 1bpp R + 1 x 1bpp G + 1 x 1bpp B with Exposure = 8333us
9 x 8bpp G + 10 x 1bpp G + 1 x 1bpp R + 1 x 1bpp G + 1 x 1bpp B with Exposure = 10500us
Thank you,
Cole