This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey,
Our lab is gonna buy a DMD for modulating our laser beam. We want to use it for 850nm laser. The chip satisfy our requirement is DLP4500NIR, which has a wavelength range of 700-2500nm. To get the control circuit, we plan to buy the DLP® NIRscan™ Evaluation Module which actually contains a DLP4500NIR chip inside. But the wavelength range for this EVM is 1350-2450nm, which does not include the 850nm. I wonder if it is caused by the light source inside the EVM (if it has). Can we still use it to modulate the 850nm laser if we remove the light source? Thank you very much!
Junling