This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need 2 MBMC sequences:
7 x 1bpp G + 1 x 1bpp R + 1 x 1bpp B + 40 x 1bpp G with Exposure = 16666us
7 x 1bpp G + 1 x 1bpp R + 1 x 1bpp B + 40 x 1bpp G with Exposure = 20000us
The sequences are 49 1bpp frames, with all green frames, except for frame 8 and 9 which are red and blue respectively.
The only difference between the sequences are the exposure times which is 16666 for the first sequence and 20000 for the second sequence.
BTW, when configuring a standard pattern sequence, we have the "exposure" and "trigger period" settings. The exposure is always at least 330us below the trigger period, but it is the trigger period that sets the frame rate, right?
The exposure times I'm requesting should produce a frame rate of 50Hz and 60Hz. If that is not the case, then I need the exposure times to be reduced by 330us so that the actual period is 16666 and 20000, with the exposure being as large as possible inside that frame period.
Thanks,
Hi Paulo
These sequences should be posted at the following link within the next 24 hours.
http://software-dl.ti.com/dlp/embedded/catalog/dlp3000/dlp3000mbmc.html
Thanks,
Clinton