This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC350 internal buffer

Genius 5960 points

Hi,

I am a previous following questions.

e2e.ti.com/.../403806

I tried the following pattern.

1bit 16 sheets + 8bit 4 sheets → NG   ex) Attach the setting screen of the GUI.
1bit 16 sheets + 8bit 3 sheets → OK
1bit 17 sheets + 8bit 3 sheets → NG
1bit 16 sheets + 6bit 4 sheets → NG
1bit 16 sheets + 6bit 3 sheets → OK

In the case of OK, it can be displayed properly.

In the case of NG, You can display, but it is not a normal image.

I want to know the combination of projection propriety.

Could you tell me if there is a combination of the law?

Best Regards,

hamada

  • Hi Hamada-san,

    There is no restriction or combination law as such. It should display properly. Please explain what do you mean by 'not normal image'...

    For example: 1bit 16 sheets + 8bit 4 sheets → NG
    Can you describe how the images are stored ? Where the images are stored in the flash, Flash index - 0,1,...

    Regards,
    Sanjeev
  • Hi,Sanjeev.

    I'm sorry.
    It was confirmed again for the "NG".
    In the case of "NG", "Pattern Number OOR" did not display lights.


    I want to know is the law of combination that can be projected.

    Best Regards,
    hamada
  • Hi,

    please reply.

    Best Regards,
    hamada
  • Please explain => "Pattern Number OOR" did not display lights.
    I tried your settings with v3.0 REL build firmware, i have used S1 and S2 Flash Index images. It displayed properly.

    1bit 16sheet + 8bit 4 sheets as follows:
    S1 - G0-G7 R0-R7 1bit 16 sheets
    S1 B7:0 8bit 1 sheet
    S2 G7:0 8bit 1 sheet
    S2 R7:0 8bit 1 sheet
    S2 B7:0 8bit 1 sheet


    Regards,
    Sanjeev