This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti experts,
I have a problem with "play once" in "Pattern Sequence" mode.
(1)
- I use GUI v3.0.1.
- Data streamed throught HDMI port in 60hz.
(2)
My setting in GUI (attached) :
- Operating Mode = Pattern sequence
- Pattern Exposure = Pattern Perdiod = 13000 (us)
- Pattern Source = Video port
- Trigger Mode = Vsync
- Clear DMD after exposure unchecked
- 3 8bit depth patterns are added to pattern sequence.
Q)
I expect that it displays only one during 3X(Pattern Exposure).
It displays about six times ! I can't understand why ?
If Pattern Exposure (= Pattern Perdiod) is set to high values (1000000 for example) it displays only one.
If I add 12 8bit depth pattern (or more) to the pattern sequence, it displays only one.
The question is : how can I get only one display during 39000us ?
Regards,
Ahmed