This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLIGHTCRAFTER: HDMI external streaming pattern sequence

Part Number: DLPLIGHTCRAFTER

I cannot detect the out trigger signal when using the "HDMI external streaming pattern sequence".However, I have been using the stored pattern with the output trigger signal to synchronize my cameras. Is there any difference between the two? Or how can I successfully syc my cameras in the  "HDMI external streaming pattern sequence" model?

Because the User's Guide says: The output trigger can only be enabled if the EVM is in either "Stored Pattern Sequence" mode or "External Streaming Pattern Sequence" while in "HDMI Port" mode. So there must be some way to generate trigger outwards.