Hi,
I use the DLPDLCR3010EVM-G2 tool with the GUI DLP Lightcrafter Display v7.0.
It seems I cannot change the splash images, even when using the resolution advised to Arturo. I tried .jpg and .png formats.
I can only project the first splash image (replacing the logo splash), but never any other splash image. The EVM becomes slow. Furthermore, when going to the Advanced tab, under Splash section, and clicking on Read Splash Screen Header, I get the following error message: Read Cmd:SplashScreenHeader, addr;37, subAddr:f SendRead(FAILED(1)). This seems to indicate that even though I can project one image, the procedure did not go well.
Could you please give more information on how to project multiple splash images with this tool: precise resolution in pixels, precise format, precise procedure?
Thank you very much,
Emmanuel