Other Parts Discussed in Thread: DLPC350,
Hi,
I have an issue with uploading firmware to my DLP4500 and I get a prompt of '' Unable to get flash manufacture ID'' . I have tried previous solutions suggested for the issue , but none of these have worked for my case. As soon as the firmware tries to upload, in the device manager , the DLPC350 turns into an unspecified device, and the green button stops flashing on the EVM. I have tried with other USB cables as well, same issue.
But the firmware uploads, and the device works perfectly on one of my colleagues laptop. The only difference I have noticed between the device functions in the device manager properties for the DLPC350 is that, in his system, it shows an extra function of "HID-compliant vendor-defined device" as a Human Interface Device.
Please help out with this at the earliest.
Regards,
Nikhil