I am unable to upload firmware to the LightCrafter 4500, I get the error "Unable to read flash manufacturer ID." I get this error when using both the GUI and the TI 3D Scanner software described here:
http://www.ti.com/lit/ug/dlpu019/dlpu019.pdf
I was able to successfully upload firmware the first few times I attempted it, then the error began. I am familiar with the following two posts on the subject, but the solutions either don't seem to apply to me (I'm not using I2C) or they don't work (I've tried multiple USB ports, etc):
http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/t/309183
http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/t/351192
My computer is running Windows 8.1 and the LightCrafter 4500 is connected via USB & HDMI.
So far I've tried:
- Different USB ports
- Removing the USB extension cable from the system
- Using compressed air to blow out USB cables
- Uninstalling & reinstalling USB composite device drivers
- "Load Default Configuration" in the GUI
- Loading the default flash image (as opposed to one with an additional flash image) - still won't load
- Clicking the "Reset System" button in the GUI
- Verifying the presence of the FlashManufacturerID.txt file in the same folder as the .exe (it's there)
- Swapping the LightCrafter 4500 motherboard with one from another unit we have (I had to keep the same light engine since it's been modified)
- I should add I've carefully checked to make sure the cables are connected properly after the swap
I have NOT tried:
- A different PC
- I can try this as a troubleshooting step, but eventually I'll need the LightCrafter to work with the PC it's connected to now due to specialized software that's installed on it.
- Replacing the USB cable
Does anyone have insight into this problem? I need to find a solution before I can move forward.