This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR6500EVM: Triggering

Part Number: DLPLCR6500EVM

Hello,

I just need some clarification on triggering my DLP using an external source. If I put a jumper over J19 pin 1-2 for using 3.3V, I wouldn't need a voltage supply for J20 through pin 1, right?

Also, I don't quite understand this statement in the EVM manual: "The trigger inputs on J20 are inputs from external devices to control the pattern sequence. While trigger input 2 is high, trigger input 1 will advance the pattern sequence to the next pattern in the sequence on every pulse". If I am only using trigger input 1, why do I need to keep trigger input 2 high?

Thanks in advance.