This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DLPDLCR2000EVM: DLPDLCR2000EVM / Raspberry pi 3 b +

Part Number: DLPDLCR2000EVM

Tool/software: Linux

(attention my english is not very good) i'm french

Hello, I allow myself to come to you because my display on raspberry p13 + is unstable. I have everything installed as explained. I modified the config.txt file. The display on the projector only appears when I type these lines
sudo i2cset -y 3 0x1b 0x0c 0x00 0x00 0x00 0x13 i
sudo i2cset -y 3 0x1b 0x0b 0x00 0x00 0x00 0x00 i
I also put these lines in the /etc/rc.local file

I do not have the display on the projector at the start of the raspberry and nothing when I play a video.
But the poster appears 1 minute and then disappears. Do you have a solution.