This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: LightCrafter 4500 Long Throw IR projection option

Part Number: DLP4500

Hello, our group is currently using LightCrafter4500 on our test bench for 3D depth reading. However we wish to switch to IR illumination as well as change the lens or possibly the light engine to produce much longer throw ratio to cover a smaller image size at our operating distance of 100mm. we need a 1.5 times narrower angle than the one we get with lightcrafter 4500. are there additional options for lens switching and possibly non visible illumination for lightcrafter 4500?

  • Dear Merrymel

    EKB Technologies offers an IR version for LightCrafter 4500 called IR E4500 MKII. As part of the E4500 Series we have a long throw option for IR variant as well. Our standard long throw is 1.8 which should fit your system based
    on your description. you can find additional details on our eStore at:

  • Dear merrymel

    EKB Technologies offers an IR version for LightCrafter 4500 called IR E4500 MKII. As part of the E4500 Series we have a long throw option for IR variant as well. Our standard long throw is 1.8 which should fit your system based
    on your description. you can find additional details on our eStore at:

  • Hi Meerymel,

    TI doesn't offer a stock EVM specifically for IR applications. Please check out the third-party solution mentioned by Abhijit.

    Regards

    Azad