This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DLP2010EVM-LC
Hi user,
Can you please share the version of GUI you are using, it would be nice if you can share the screen shot of the GUI.
Thanks,
Navneet
Hi user,
Have you installed the driver cypress driver ?
At the time of GUI installation, one window ask for installing the cypress driver. Please check that you have correctly installed the cypress driver.
You can validate the driver by checking in your system's device manager
Thanks,
Navneet
Hi User,
Can you please let me know what all LED's are on, when SW1 is on.
Can you please do one experiment for us, start the EVM first, then open the GUI. Observe the LED behavior on the EVM. When you start the GUI, this sequence should happen :
D11 off -> D9 on -> D8 on -> D11 blink (on-off) -> D9 and D8 off, D11 on
Thanks,
Navneet
Hi Zong,
Looks like MSP430_REQ is sending to Cypress chip but it is not acknowledge back on MSP430_ACK.
we need to debug the cypress chip, can you please see if there is any activity going on this signal "USB_IIC0_SCL" Also please check what is the status of "SW_ONOFF"
Can you re-program the MSP430 code in your EVM. It is available here : http://www.ti.com/tool/DLP2010EVM-LC
I hope reprogramming the MSP430 code solve this issue. If doesn't, then we need to debug the cypress chip.
Thanks,
Navneet