This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC: Can this do 1440Hz 1-bit patterns or not?

Part Number: DLP3010EVM-LC

Dear TI,

Can you kindly confirm directly if the DLP3010EVM-LC can do 1440Hz 1-bit patterns from a 60Hz 24-bit external feed?

I have been trying to use the GUI tool to configure this but the UI doesn't want to play ball.

I was really hopeful that an EVM built nearly 8 years after the DLP-Pico v2 would be trivially easy to configure in the same way the Pico did, (4 commands over I2C and it would be purring away like a kitten delivering 1440Hz 1-bit), but I am finding the new kit frustratingly hard to work with.

Thanks.

Abe

  • Hi Abe,

    Yes, this EVM supports 1-bit 1440 Hz over external video. Can you please explain what issue you're facing?

    Regards

    Azad

  • Hi Azad,

    We have an external video stream (which is bit-packed as 24-bit 60 Hz frames) and we would like to command the kit to output this as 1440Hz 1-bit monochrome frames.

    We are using DLPComposer.LightCrafter.exe v2.1.0.7 to set the output mode.

    However, in the Light Control panel, we are not able to set framerate at times (sometimes it defaults to 120Hz  and disabled),

    If it gets set somehow, the software is forcing us to set the pre-exposure dark time, exposure time and post-exposure dark times as values that are too large

    We do not need pre/post exposure times. We also don't need "exposure" time per se, but I can understand that this may need to be set (I am not sure if this should be set to 1000000/1440 = 694us)

    Can you help us sort this problem out?

    Thanks.

    Regards,

    Abe

  • Hi Abe,

    The Frame Rate cannot be set directly, the GUI calculates the Frame Rate based on the exposure and dark times provided by the user.

    Note that dark times are required, this EVM cannot project patterns without pre-exposure and post-exposure dark times. For more information refer to this FAQ: 

    For 1-bit 1440 Hz, the sum of exposure and dark times should be 694us. The timings in this case would be 197/462/35 us (pre-dark/exposure/post-dark).

    Regards

    Azad

  • Hi Azad,

    I will give this a try. While the dark time is not ideal, but we can try to work with it.

    Thanks.

    Abe

  • Hi Azad,

    Yes, that worked great. However, I am not able to figure out the order of bit-packing.

    Is it R0-7,G0-7,B0-7?

    Thanks.

    Abe

  • Hi Abe,

    It's B0-7, G0-7, R0-7.

    Regards

    Azad

  • Hi Azad,

    Thanks for the help.

    Regards,

    Abe