This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP480RE: Looking for DMD with part number 1912-1132

Part Number: DLP480RE


Hi E2E,

Good day.

We have a customer looking for the TI DarkChip 3 DMD with Resolution of 1920x1200 and a size of 0.95inch, with part number 1912-1132. The closest component that we found was DLP480RE which has a DMD part number of 1912-513AB. Refer to the section 11.1.2 Device Markings on the datasheet.
DLP480RE datasheet: http://www.ti.com/lit/ds/symlink/dlp480re.pdf

Is the DMD with part number 1912-1132 is indeed DLP480RE? and that the “513AB” is an assembly related changes only? Is there a PCN that support this and can we provide this to the customer?

Appreciate your support on this.

Art