Hi
I am Designing a projector using DLPC350,
based on table 20 the MAXIMUM SIGNAL ROUTING LENGTH is 75mm.
but in lightcrafter4500 eval board this total trace length is more than 90mm.
and I have problem in PCB design since the flex cable trace length is around 52mm and if I use DMD FQE package the internal trace is around 8mm
means I have only 15mm on my PCB board.
is it correct? how much I can increase the total trace length without any problem.