This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPNIRNANOEVM: NIR Spectrum range below 900nm

Part Number: DLPNIRNANOEVM


Hi DLP Experts,

Our customer is interested in taking infrared measurements between 700 to 1700nm. We have looked at the DLPNIRNANOEVM, and although the DMD chip supports operation at wavelengths between 700 to 2500 nm, the EVM is restricted at 900 to 1700 nm. I understand that this may be part of the detector restrictions and the rest of the system design around the DMD. Can you help on possible solutions on how can our customer implement this? Thanks in advance for the help.

Regards,

Jejomar