Other Parts Discussed in Thread: DLP2010NIR, DLPC150
if I buy the DLP2010NIR's evaluation module (the one with the spectrometer inside), am I able to remove the spectrometer from the module, or remove the light source with a light beam from a source of our own (a light beam coming outside of the module)? And I also noticed that the DMD board is controlled by the DMD controller, so are there separable? I could buy extension cables, but just wondering if there is any physical attachment between these two, so that they are not separable?